ModelingViewHighQualityImageDisplayTechniqueType Enumeration¶
NXOpen.ModelingViewHighQualityImage.DisplayTechniqueType is an alias for NXOpen.ModelingViewHighQualityImageDisplayTechniqueType
-
class
NXOpen.
ModelingViewHighQualityImageDisplayTechniqueType
¶ Bases:
object
Describes the technique to be used when generating the High Quality Image
Enum Members
random noise to the initial RGB values before the dither takes place. “
“FsRgb”, ” The pixel conversion process uses the Floyd-Steinberg ditheralgorithm to distribute the color error across the picture. This is a recommended mode for 8 bit plane display devices. “
“FsRgbPlusNoise”, ” The Floyd-Steinberg algorithm is augmented with the additionof random noise to the initial RGB values before the dither takes place. For some images this method avoids artifacts that can occur using the FS RGB method. “
“Monochrome”, ” Pixels are converted to black and white and dithered usingthe Floyd-Steinberg algorithm. This mode is useful on 1 bit display devices. “
“GrayScale”, ” Each pixel is converted to a gray level using the NTSC color- to gray scale conversion. “
- “NearestRgb”, ” Conversion is to the nearest RGB value in the color lookup table. ” “OrderedDither”, ” A color dither matrix screens pixel colors. This is a trade of
color resolution for screen resolution. This method is faster then the Floyd-Steinberg dither methods but tends to introduce a noticeable pattern in the output image. “
“TcPlusNoise”, ” Random noise is added to each pixel where the noise isspecifically tailored for true color display devices. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.