SketchOffsetBuilder Class¶
-
class
NXOpen.
SketchOffsetBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchOffsetBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchOffsetBuilder()
Default values.
Property Value CapType Extension ConvertToReference False CreateDimension True Degree 3 Distance.Value 5.0 (millimeters part), 2.0 (inches part) IsSymmetric False NumberOfCopies 1 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CapType | Returns or sets the type of the cap needed at the corners |
ConvertToReference | Returns or sets the flag to indicate if the input curves needs to converted to reference |
CreateDimension | Returns or sets the flag to create offset with a dimension or a dimensionless offset |
Degree | Returns or sets the degree for approximating offset spline |
Distance | Returns the offset distance expression |
IsSymmetric | Returns or sets the flag to indicate if the offset needs to be symmetric or not |
NumberOfCopies | Returns or sets the number of offset copies |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance for approximating offset spline |
Methods¶
Method | Description |
---|---|
BreakChain | This function breaks the base chain and all the associated offsets at a given location |
Commit | Commits any edits that have been applied to the builder. |
CreateSection | The function creates a new empty section object and adds it to the builder @return New section object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EvaluateOffset | This function will solve the offset constraint to update it based on the new data set in the builder |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOutputCurvesOfOffset | This function gets all output curves of an offset @return All the curves associated with constraint |
GetSections | This function gets all sections of an offset during create/edit @return All the sections associated with the builder |
MergeChains | This function merges the two chains. |
RemoveSection | The function removes the given section from the builder |
ReverseOffsetDirectionOfChain | This function reverses the offset direction of the chain containing the input geometry |
SetEndConstraint | This function removes end constraint from the given offset |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateLoopsAndCopies | This function will update the offset after curves are selected. |
UpdateSolverDistance | This function will update the distance in the sketch solver using the new data set in the builder |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CapType¶
-
SketchOffsetBuilder.
CapType
¶ Returns or sets the type of the cap needed at the corners
-------------------------------------
Getter Method
Signature
CapType()
Returns: Return type: NXOpen.SketchOffsetCapType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CapType(capType)
Parameters: capType ( NXOpen.SketchOffsetCapType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
ConvertToReference¶
-
SketchOffsetBuilder.
ConvertToReference
¶ Returns or sets the flag to indicate if the input curves needs to converted to reference
-------------------------------------
Getter Method
Signature
ConvertToReference()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConvertToReference(reference)
Parameters: reference (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateDimension¶
-
SketchOffsetBuilder.
CreateDimension
¶ Returns or sets the flag to create offset with a dimension or a dimensionless offset
-------------------------------------
Getter Method
Signature
CreateDimension()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateDimension(createDim)
Parameters: createDim (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Degree¶
-
SketchOffsetBuilder.
Degree
¶ Returns or sets the degree for approximating offset spline
-------------------------------------
Getter Method
Signature
Degree()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Degree(degree)
Parameters: degree (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Distance¶
-
SketchOffsetBuilder.
Distance
¶ Returns the offset distance expression
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
IsSymmetric¶
-
SketchOffsetBuilder.
IsSymmetric
¶ Returns or sets the flag to indicate if the offset needs to be symmetric or not
-------------------------------------
Getter Method
Signature
IsSymmetric()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSymmetric(symmetric)
Parameters: symmetric (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
NumberOfCopies¶
-
SketchOffsetBuilder.
NumberOfCopies
¶ Returns or sets the number of offset copies
-------------------------------------
Getter Method
Signature
NumberOfCopies()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberOfCopies(copies)
Parameters: copies (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Tolerance¶
-
SketchOffsetBuilder.
Tolerance
¶ Returns or sets the tolerance for approximating offset spline
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Method Detail¶
BreakChain¶
-
SketchOffsetBuilder.
BreakChain
¶ This function breaks the base chain and all the associated offsets at a given location
Signature
BreakChain(object1, object2, helpPt)
Parameters: - object1 (
NXOpen.NXObject
) – An object in chain to break - object2 (
NXOpen.NXObject
) – Adjacent object to the previous one - helpPt (
NXOpen.Point3d
) – Help point for multiple intersections
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
- object1 (
CreateSection¶
-
SketchOffsetBuilder.
CreateSection
¶ The function creates a new empty section object and adds it to the builder
Signature
CreateSection()
Returns: New section object Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
EvaluateOffset¶
-
SketchOffsetBuilder.
EvaluateOffset
¶ This function will solve the offset constraint to update it based on the new data set in the builder
Signature
EvaluateOffset()
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
GetOutputCurvesOfOffset¶
-
SketchOffsetBuilder.
GetOutputCurvesOfOffset
¶ This function gets all output curves of an offset
Signature
GetOutputCurvesOfOffset()
Returns: All the curves associated with constraint Return type: list of NXOpen.NXObject
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
GetSections¶
-
SketchOffsetBuilder.
GetSections
¶ This function gets all sections of an offset during create/edit
Signature
GetSections()
Returns: All the sections associated with the builder Return type: list of NXOpen.Section
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
MergeChains¶
-
SketchOffsetBuilder.
MergeChains
¶ This function merges the two chains.
The last geom of first chain and first geom of next chain are taken as input.
Signature
MergeChains(object1, object2, helpPt)
Parameters: - object1 (
NXOpen.NXObject
) – Last geom of first chain - object2 (
NXOpen.NXObject
) – First geom of next chain - helpPt (
NXOpen.Point3d
) – Help point for multiple intersections
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
- object1 (
RemoveSection¶
-
SketchOffsetBuilder.
RemoveSection
¶ The function removes the given section from the builder
Signature
RemoveSection(section)
Parameters: section ( NXOpen.Section
) – Section obj to removeNew in version NX5.0.0.
License requirements: None.
ReverseOffsetDirectionOfChain¶
-
SketchOffsetBuilder.
ReverseOffsetDirectionOfChain
¶ This function reverses the offset direction of the chain containing the input geometry
Signature
ReverseOffsetDirectionOfChain(objectInChain)
Parameters: objectInChain ( NXOpen.NXObject
) – An object in chain to reverseNew in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
SetEndConstraint¶
-
SketchOffsetBuilder.
SetEndConstraint
¶ This function removes end constraint from the given offset
Signature
SetEndConstraint(objectInChain, inx, isStartEnd, constraint)
Parameters: - objectInChain (
NXOpen.NXObject
) – An object in the base chain - inx (int) – Index of the constraint - starts from 0
- isStartEnd (bool) – TRUE, if we want to remove the start end con
- constraint (bool) – TRUE to add the con, false to remove
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
- objectInChain (
UpdateLoopsAndCopies¶
-
SketchOffsetBuilder.
UpdateLoopsAndCopies
¶ This function will update the offset after curves are selected.
If the input section is updated to add/remove curves, this function must be called to update the offset constraint. This function will keep the offset constraint synchronised with the edits done to input section.
Signature
UpdateLoopsAndCopies()
New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
UpdateSolverDistance¶
-
SketchOffsetBuilder.
UpdateSolverDistance
¶ This function will update the distance in the sketch solver using the new data set in the builder
Signature
UpdateSolverDistance()
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Validate¶
-
SketchOffsetBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.