SubdivisionTaskEnvironment Class¶
-
class
NXOpen.
SubdivisionTaskEnvironment
¶ Bases:
object
Represents the subdivision task environment associated with a session.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveSubdivisionBodyFeature | Returns the active subdivision body feature. |
Methods¶
Method | Description |
---|---|
Enter | Starts subdivision task environment. |
Exit | Ends subdivision task environment. |
SetCancelled | Marks the task to be cancelled such that during SubdivisionTaskEnvironment.Exit() task is undone and all the changes are discarded. |
SetFeatureToEdit | Sets the feature to be edited. |
Property Detail¶
ActiveSubdivisionBodyFeature¶
-
SubdivisionTaskEnvironment.
ActiveSubdivisionBodyFeature
¶ Returns the active subdivision body feature.
-------------------------------------
Getter Method
Signature
ActiveSubdivisionBodyFeature()
Returns: Return type: NXOpen.Features.Subdivision.SubdivisionBody
New in version NX9.0.0.
License requirements: None.
Method Detail¶
Enter¶
-
SubdivisionTaskEnvironment.
Enter
¶ Starts subdivision task environment.
This method should be called before starting to use subdivision body feature tools. This method should not be called if already in a subdivision task environment.
Signature
Enter()
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
Exit¶
-
SubdivisionTaskEnvironment.
Exit
¶ Ends subdivision task environment.
Signature
Exit()
New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SetCancelled¶
-
SubdivisionTaskEnvironment.
SetCancelled
¶ Marks the task to be cancelled such that during
SubdivisionTaskEnvironment.Exit()
task is undone and all the changes are discarded.Signature
SetCancelled()
New in version NX11.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)
SetFeatureToEdit¶
-
SubdivisionTaskEnvironment.
SetFeatureToEdit
¶ Sets the feature to be edited.
Signature
SetFeatureToEdit(subdivisionBodyFeature)
Parameters: subdivisionBodyFeature ( NXOpen.Features.Subdivision.SubdivisionBody
) –New in version NX9.0.0.
License requirements: nx_subdivision (” NX SUBDIVISION”)