AttributePropertiesBaseBuilderBooleanValueOptions Enumeration¶
NXOpen.AttributePropertiesBaseBuilder.BooleanValueOptions is an alias for NXOpen.AttributePropertiesBaseBuilderBooleanValueOptions
-
class
NXOpen.
AttributePropertiesBaseBuilderBooleanValueOptions
¶ Bases:
object
The value choices for an attribute of type Boolean
Enum Members
Enum Member Enum Member Description False FalseTrue True-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-