ScalarCollection Class¶
-
class
NXOpen.
ScalarCollection
¶ Bases:
object
Represents a collection of
NXOpen.Scalar
objects.Iterating this collection only returns live uncondemned objects contained in the owning part of the collection. Note that
NXOpen.Scalar
is a smart object and many smart objects are condemned as they only exist to support other objects and are not displayed. Condemned objects will be deleted when their references go away. To obtain an instance of this class, refer toNXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateScalar | Creates a scalar without parameters. |
CreateScalarExpression | Creates a scalar using an expression. |
CreateScalarReciprocalValue | Creates a scalar whose value is a reciprocal of another scalar @return |
Method Detail¶
CreateScalar¶
-
ScalarCollection.
CreateScalar
¶ Overloaded method CreateScalar
CreateScalar(value, dimensionality, update)
CreateScalar(scalarExtract, scalarOptional, dimensionality, update)
-------------------------------------
Creates a scalar without parameters.
Signature
CreateScalar(value, dimensionality, update)
Parameters: - value (float) –
- dimensionality (
NXOpen.ScalarDimensionalityType
) – - update (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
Creates a scalar via an existing scalar and an optional scalar.
Signature
CreateScalar(scalarExtract, scalarOptional, dimensionality, update)
Parameters: - scalarExtract (
NXOpen.Scalar
) – - scalarOptional (
NXOpen.Scalar
) – - dimensionality (
NXOpen.ScalarDimensionalityType
) – - update (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
-------------------------------------
CreateScalarExpression¶
-
ScalarCollection.
CreateScalarExpression
¶ Creates a scalar using an expression.
Signature
CreateScalarExpression(expression, dimensionality, update)
Parameters: - expression (
NXOpen.Expression
) – - dimensionality (
NXOpen.ScalarDimensionalityType
) – - update (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX3.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- expression (
CreateScalarReciprocalValue¶
-
ScalarCollection.
CreateScalarReciprocalValue
¶ Creates a scalar whose value is a reciprocal of another scalar
Signature
CreateScalarReciprocalValue(scalar, dimensionality, update)
Parameters: - scalar (
NXOpen.Scalar
) – - dimensionality (
NXOpen.ScalarDimensionalityType
) – - update (
NXOpen.SmartObjectUpdateOption
) –
Returns: Return type: New in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
- scalar (