SketchConstraintClass Enumeration¶
NXOpen.Sketch.ConstraintClass is an alias for NXOpen.SketchConstraintClass
-
class
NXOpen.
SketchConstraintClass
¶ Bases:
object
Represents the class of the constraint.
There are two classes of constraints: geometric and dimension
Enum Members
- to select both types of constraints “
- “Geometric”, ” A non-dimension constraint ” “Dimension”, ” A dimensional constraint “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.