SmartObjectVisibilityOption Enumeration¶
NXOpen.SmartObject.VisibilityOption is an alias for NXOpen.SmartObjectVisibilityOption
-
class
NXOpen.
SmartObjectVisibilityOption
¶ Bases:
object
Specifies the smart object visibility.
Enum Members
Enum Member Enum Member Description Invisible Default creation.Visible VisibleIfParentInvisible Visible if a parent is not loaded (for extract).-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-