CurveFeatureTangentRule Class¶
-
class
NXOpen.
CurveFeatureTangentRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects tangent connected curves from the feature of the seed.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the curve feature tangent rule: NXOpen.CurveFeatureTangentRule |
Method Detail¶
Dispose¶
-
CurveFeatureTangentRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
CurveFeatureTangentRule.
GetData
¶ Gets the data for the curve feature tangent rule:
NXOpen.CurveFeatureTangentRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (features, seedCurve, endCurve, isFromSeedStart, angleTolerance, gapTolerance). features is a list of
NXOpen.Features.Feature
. Feaures whose tangent curves are used to create this ruleseedCurve is aNXOpen.Curve
. Seed curve endCurve is aNXOpen.Curve
. End curve. It can be null (Nothing) isFromSeedStart is a bool. True: the chain starts from the start point of the seed curve angleTolerance is a float. Angle tolerance for tangent curves gapTolerance is a float. Gap tolerance for tangent curves .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)