DateItemBuilder Class¶
-
class
NXOpen.
DateItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class stores a date and time.
The class does verify that the year string and time string are in a valid format. The first date supported is 2-Jan-1900 00:00:00 UTC and the last date supported is 31st-Dec-9999 00:00:00 UTC. Though note that the time input is in local time and converted to UTC internally.
NOTE: The class does NOT verify that the combination of day, month, year and time is valid.
To create a new instance of this class, use
NXOpen.DateBuilder.CreateDateItemBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Day | Returns or sets the day |
Month | Returns or sets the month |
Tag | Returns the Tag for this object. |
Time | Returns or sets the time. |
Year | Returns or sets the year. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DateItemBuilderDayOfMonth Enumeration | Days of the month |
DateItemBuilderMonthOfYear Enumeration | Months of the year. |
Property Detail¶
Day¶
-
DateItemBuilder.
Day
¶ Returns or sets the day
-------------------------------------
Getter Method
Signature
Day()
Returns: Return type: NXOpen.DateItemBuilderDayOfMonth
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Day(day)
Parameters: day ( NXOpen.DateItemBuilderDayOfMonth
) –New in version NX8.0.0.
License requirements: None.
Month¶
-
DateItemBuilder.
Month
¶ Returns or sets the month
-------------------------------------
Getter Method
Signature
Month()
Returns: Return type: NXOpen.DateItemBuilderMonthOfYear
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Month(month)
Parameters: month ( NXOpen.DateItemBuilderMonthOfYear
) –New in version NX8.0.0.
License requirements: None.
Time¶
-
DateItemBuilder.
Time
¶ Returns or sets the time.
The time string is a 24-hour clock time in the format HH:MM:SS or HH:MM. The string can also be empty.
-------------------------------------
Getter Method
Signature
Time()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Time(time)
Parameters: time (str) – New in version NX8.0.0.
License requirements: None.
Year¶
-
DateItemBuilder.
Year
¶ Returns or sets the year.
The year string is four characters long and represents an integer within the range minimum year and maximum year (inclusive). The year can also be an empty string.
-------------------------------------
Getter Method
Signature
Year()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Year(year)
Parameters: year (str) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DateItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.