BasePartCloseModified Enumeration¶
NXOpen.BasePart.CloseModified is an alias for NXOpen.BasePartCloseModified
-
class
NXOpen.
BasePartCloseModified
¶ Bases:
object
Indicates how part close should handle component parts when they are modified
Enum Members
NXOpen.PartCloseResponses
to determine whether to close a modified part or not ““CloseModified”, ” Close all modified parts ” “DontCloseModified”, ” Do not close any modified parts “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-