ColorDefinition Class¶
-
class
NXOpen.
ColorDefinition
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.ColorDefinition
, which is a representation of one color on an NX color palette.Each color has an index into the palette, a name, rgb values, and an optional favorite index.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ColorIndex | Returns or sets the color index. |
ColorName | Returns or sets the color name. |
FavoriteIndex | Returns or sets the favorite index. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetColorValues | Gets the color values. |
SetColorValues | Sets the color values. |
Property Detail¶
ColorIndex¶
-
ColorDefinition.
ColorIndex
¶ Returns or sets the color index.
This is an number ranging from 0 to 216, each color on the color palette must have a unique index.
-------------------------------------
Getter Method
Signature
ColorIndex()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorIndex(colorIdx)
Parameters: colorIdx (int) – New in version NX5.0.0.
License requirements: None.
ColorName¶
-
ColorDefinition.
ColorName
¶ Returns or sets the color name.
-------------------------------------
Getter Method
Signature
ColorName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorName(colorName)
Parameters: colorName (str) – New in version NX5.0.0.
License requirements: None.
FavoriteIndex¶
-
ColorDefinition.
FavoriteIndex
¶ Returns or sets the favorite index.
The favorite index is a unique number between 0 and 29 specifing the index into the favorite color array. If the color is not a favorite, it has an index of -1.
-------------------------------------
Getter Method
Signature
FavoriteIndex()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FavoriteIndex(favoriteIdx)
Parameters: favoriteIdx (int) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetColorValues¶
-
ColorDefinition.
GetColorValues
¶ Gets the color values.
This is an array of 3 doubles containing the RGB values of the color.
Signature
GetColorValues()
Returns: Return type: NXOpen.ColorDefinitionRgb
New in version NX5.0.0.
License requirements: None.
SetColorValues¶
-
ColorDefinition.
SetColorValues
¶ Sets the color values.
This is an array of 3 doubles containing the RGB values of the color.
Signature
SetColorValues(colorVals)
Parameters: colorVals ( NXOpen.ColorDefinitionRgb
) –New in version NX5.0.0.
License requirements: None.