SelectionUistylerSelectionType Enumeration¶
NXOpen.Selection.UistylerSelectionType is an alias for NXOpen.SelectionUistylerSelectionType
-
class
NXOpen.
SelectionUistylerSelectionType
¶ Bases:
object
Indicates the general class of object to filter selection.
Enum Members
- this function is called again “
- “SingleSelection”, ” allows
- single select “
- “SingleDeselection”, ” single deselect ” “RobustSelection”, ” reselect last ” “SinglePosition”, ” the position is returned if no object is selected with the
- single select gesture “
- “RectanglePosition”, ” the position is returned if no object is selected with the
single select gesture “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.