SketchCreateDimensionOption Enumeration¶
NXOpen.Sketch.CreateDimensionOption is an alias for NXOpen.SketchCreateDimensionOption
-
class
NXOpen.
SketchCreateDimensionOption
¶ Bases:
object
Used in fillet to indicate whether a radius dimension should be created by the fillet
Enum Members
Enum Member Enum Member Description False Do not create a radius dimensionTrue Create a radius dimension-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-