JournalManager Class¶
-
class
NXOpen.
JournalManager
¶ Bases:
object
Represents the JournalManager which is used to query data about journals when recording and replaying journal files.
The language NX is setup to, or currently recording can be determined from
NXOpen.Preferences.SessionUserInterface.JournalLanguage()
.To obtain an instance of this class, refer to
NXOpen.Session
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
JournalLanguage |
|
Methods¶
Property Detail¶
JournalLanguage¶
-
JournalManager.
JournalLanguage
¶ Returns the language the journal will be recored in.
This is a convenience querry, as this will return the same value as
NXOpen.Preferences.SessionUserInterface.JournalLanguage()
-------------------------------------
Getter Method
Signature
JournalLanguage()
Returns: Return type: NXOpen.Preferences.SessionUserInterfaceJournalLanguageType
New in version NX11.0.0.
License requirements: None.