SessionUserInterfaceJournalLanguageType Enumeration

NXOpen.Preferences.SessionUserInterface.JournalLanguageType is an alias for NXOpen.Preferences.SessionUserInterfaceJournalLanguageType

class NXOpen.Preferences.SessionUserInterfaceJournalLanguageType

Bases: object

Describes the language used to record journals

Enum Members

Enum Member Enum Member Description
VisualBasic
CPlusPlus
C++ restricts the file format to Ascii
Java
Cs
Python
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.