FaceBodyRule Class¶
-
class
NXOpen.
FaceBodyRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all the faces of a body.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetBodyData | Gets the data for the face body rule: NXOpen.FaceBodyRule @return Body which creates this rule |
Method Detail¶
Dispose¶
-
FaceBodyRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetBodyData¶
-
FaceBodyRule.
GetBodyData
¶ Gets the data for the face body rule:
NXOpen.FaceBodyRule
Signature
GetBodyData()
Returns: Body which creates this rule Return type: NXOpen.Body
New in version NX5.0.0.
License requirements: gateway (“UG GATEWAY”)