SketchConstraintVisibility Enumeration¶
NXOpen.Sketch.ConstraintVisibility is an alias for NXOpen.SketchConstraintVisibility
-
class
NXOpen.
SketchConstraintVisibility
¶ Bases:
object
Indicates the visibility of the constraints The APIs that use this enum are deprecated in NX85 The
NXOpen.SketchConstraintVisibility.Some
option will behave the same as theNXOpen.SketchConstraintVisibility.All
option.Please use
NXOpen.Preferences.SessionSketch.DisplayConstraintSymbols()
andNXOpen.Preferences.SessionSketch.DisplayConstraintSymbols()
instead.Deprecated since version NX8.5.0: Please use
NXOpen.Preferences.SessionSketch.DisplayConstraintSymbols`()
Enum Members
- Equivalent to having the UI show-all-constraints and show-no-constraints toggles off “
- “All”, ” All constraints are visible “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.