OMClass Class¶
-
class
NXOpen.
OMClass
¶ Bases:
NXOpen.TaggedObject
,NXOpen.IOMName
Represents a OMClass.
This is for internal testing only.
This is a test classs.
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Superclass | Returns the superclass |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CompareWith | Compare with @return |
GetAllAttributeInfo | Return all @return |
GetAttributes | Return the @return |
GetObjectName | Returns the object name @return |
IsDefiningClassFor | Is define @return |
Property Detail¶
Superclass¶
-
OMClass.
Superclass
¶ Returns the superclass
-------------------------------------
Getter Method
Signature
Superclass()
Returns: Return type: NXOpen.OMClass
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CompareWith¶
-
OMClass.
CompareWith
¶ Compare with
Signature
CompareWith(other)
Parameters: other ( NXOpen.IOMName
) –Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
GetAllAttributeInfo¶
-
OMClass.
GetAllAttributeInfo
¶ Return all
Signature
GetAllAttributeInfo()
Returns: Return type: list of NXOpen.OMAttributeInfo_Struct
New in version NX3.0.0.
License requirements: None.
GetAttributes¶
-
OMClass.
GetAttributes
¶ Return the
Signature
GetAttributes()
Returns: Return type: list of NXOpen.OMAttribute
New in version NX3.0.0.
License requirements: None.
GetObjectName¶
-
OMClass.
GetObjectName
¶ Returns the object name
Signature
GetObjectName()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
IsDefiningClassFor¶
-
OMClass.
IsDefiningClassFor
¶ Is define
Signature
IsDefiningClassFor(attribute)
Parameters: attribute ( NXOpen.OMAttribute
) –Returns: Return type: bool New in version NX4.0.0.
License requirements: None.