ViewDependentDisplayManagerWidth Enumeration

NXOpen.ViewDependentDisplayManager.Width is an alias for NXOpen.ViewDependentDisplayManagerWidth

class NXOpen.ViewDependentDisplayManagerWidth

Bases: object

specifies the width for wireframe edits

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
Normal  
Thick  
Thin  
Object  
One
Two
Three
Four
Five
Six
Seven
Eight
Nine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.