ExpressionCollectionImportMode Enumeration¶
NXOpen.ExpressionCollection.ImportMode is an alias for NXOpen.ExpressionCollectionImportMode
-
class
NXOpen.
ExpressionCollectionImportMode
¶ Bases:
object
Indicates the mode for importing expressions.
Enum Members
Enum Member Enum Member Description Replace Overwrite existing expressions if the imported values differDontReplace Don’t overwrite existing expressions. New expressions are createdDeleteImports Delete all expressions in the imported file-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-