PlotBuilderRotationOption Enumeration¶
NXOpen.PlotBuilder.RotationOption is an alias for NXOpen.PlotBuilderRotationOption
-
class
NXOpen.
PlotBuilderRotationOption
¶ Bases:
object
Specifies the rotation of the banner
Enum Members
Enum Member Enum Member Description Degree0 0 degree rotationDegree90 90 degree rotationDegree180 180 degree rotationDegree270 270 degree rotation-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-