ExtrudeTaperDataTaperType Enumeration¶
-
class
NXOpen.
ExtrudeTaperDataTaperType
¶ Bases:
object
This enum represents the type of taper Enum Members
Enum Member Enum Member Description NotSet No taperSimpleFromStart Simple taper from start edgesSimpleFromProfile Simple taper from profileSymmetric Symmetric taperMatchedEnds Matched end taperAsymmetric ASymmetric taper-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-