CGMBuilderOutputTextOption Enumeration¶
NXOpen.CGMBuilder.OutputTextOption is an alias for NXOpen.CGMBuilderOutputTextOption
-
class
NXOpen.
CGMBuilderOutputTextOption
¶ Bases:
object
Specifies the text option, as either text or polylines
Enum Members
Enum Member Enum Member Description Text Text is kept as textPolylines Text is exported as polylinesBestfit NX fonts are polylines, standard fonts are text-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-