EdgeVertexTangentRule Class¶
-
class
NXOpen.
EdgeVertexTangentRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects the vertex edge and the edges adjacent and tangent to it.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge vertex tangent rule: NXOpen.EdgeVertexTangentRule |
Method Detail¶
Dispose¶
-
EdgeVertexTangentRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetData¶
-
EdgeVertexTangentRule.
GetData
¶ Gets the data for the edge vertex tangent rule:
NXOpen.EdgeVertexTangentRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (startEdge, isFromStart, angleTolerance, hasSameConvexity). startEdge is a
NXOpen.Edge
. Start edge of edge tangent ruleisFromStart is a bool. True: the tangent starts from the start point of the start edge if end edge is providedangleTolerance is a float. Angle tolerance for tangent edges hasSameConvexity is a bool. True: will only find tangent edges that has the same convexity .. versionadded:: NX4.0.0License requirements: gateway (“UG GATEWAY”)