AttributeTemplatesBuilderTemplatesOptions Enumeration¶
NXOpen.AttributeTemplatesBuilder.TemplatesOptions is an alias for NXOpen.AttributeTemplatesBuilderTemplatesOptions
-
class
NXOpen.
AttributeTemplatesBuilderTemplatesOptions
¶ Bases:
object
Specifies the templates option when setting or displaying templates.
Enum Members
in customer defaults and can be managed using Import and Export. Each template in the catalog can be defined as persistent or transient. A persistent template will be copied into the part when an attribute is created. A transient template will assist in the creation of an attribute but will not be stored in the part. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-