IgesCreatorCrossHatchMapEnum Enumeration¶
NXOpen.IgesCreator.CrossHatchMapEnum is an alias for NXOpen.IgesCreatorCrossHatchMapEnum
-
class
NXOpen.
IgesCreatorCrossHatchMapEnum
¶ Bases:
object
Cross Hatch Map Option
Enum Members
Enum Member Enum Member Description SectionArea map cross hatch as section areaCopiousData map cross hatch as copious data-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-