FaceTangentRule Class¶
-
class
NXOpen.
FaceTangentRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects tangent connected faces from the body of the seed face.New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the face tangent rule: NXOpen.FaceTangentRule |
Method Detail¶
Dispose¶
-
FaceTangentRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetData¶
-
FaceTangentRule.
GetData
¶ Gets the data for the face tangent rule:
NXOpen.FaceTangentRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (startFace, endFace, isFromStart, angleTolerance, hasSameConvexity). startFace is a
NXOpen.Face
. Start face of face tangent ruleendFace is aNXOpen.Face
. End face of face tangent rule. It can be null (Nothing).isFromStart is a bool. True: the tangent starts from the start point of the start face if end face is providedangleTolerance is a float. Angle tolerance for tangent faces hasSameConvexity is a bool. True: will only find tangnet faces that has the same convexity .. versionadded:: NX4.0.0Deprecated since version NX8.0.0: This functionality is no longer supported.
License requirements: gateway (“UG GATEWAY”)