CGMBuilderWidth Enumeration¶
NXOpen.CGMBuilder.Width is an alias for NXOpen.CGMBuilderWidth
-
class
NXOpen.
CGMBuilderWidth
¶ Bases:
object
Specifies the primary selection of which type of width assignment to use.
Enum Members
Enum Member Enum Member Description StandardWidths Standard WidthsSingleWidth Single Width, uses custom widths defined in WidthDefinitionCustomThreeWidths Custom Three Widths, uses custom widths defined in WidthDefinitionCustomPalette Custom palette, uses custom widths defined in WidthDefinition-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-