HumanDataAdvancedScalingType Enumeration¶
NXOpen.HumanData.AdvancedScalingType is an alias for NXOpen.HumanDataAdvancedScalingType
-
class
NXOpen.
HumanDataAdvancedScalingType
¶ Bases:
object
This enum represents the types of the advanced scaling variable names
Enum Members
Enum Member Enum Member Description AbdominalDepth Indicate scaling of abdominal depthAcromionHeight Indicate scaling of acromion heightAnkleHeight Indicate scaling of ankle heightArmLength Indicate scaling of arm lengthBiacromialBreadth Indicate scaling of biacromial breadthBideltoidBreadth Indicate scaling of bideltoid breadthButtockKneeLength Indicate scaling of buttock_knee_lengthElbowFingertipLength Indicate scaling of elbow_fingertip_lengthElbowRestHeight Indicate scaling of elbow_rest_heightFootBreadth Indicate scaling of foot_breadthFootLength Indicate scaling of foot_lengthHandBreadth Indicate scaling of hand_breadthHandLength Indicate scaling of hand_lengthHeadBreadth Indicate scaling of head_breadthHeadHeight Indicate scaling of head_heightHeadLength Indicate scaling of head_lengthHipBreadth Indicate scaling of hip_breadthInterpupilDistance Indicate scaling of interpupil_distanceShoulderElbowLength Indicate scaling of shoulder_elbow_lengthSittingAcromialHeight Indicate scaling of sitting_acromial_heightSittingEyeHeight Indicate scaling of sitting_eye_heightSittingHeight Indicate scaling of sitting_heightSittingKneeHeight Indicate scaling of sitting_knee_heightThighClearance Indicate scaling of thigh_clearanceThumbtipReach Indicate scaling of thumbtip_reach-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-