ViewScaleAdjustment Enumeration¶
NXOpen.View.ScaleAdjustment is an alias for NXOpen.ViewScaleAdjustment
-
class
NXOpen.
ViewScaleAdjustment
¶ Bases:
object
Describes simple, predefined adjustments that may be applied to a view’s scale while another operation is performed, in conjunction, on the view.
For more details, refer to those interfaces that use this enum as a parameter.
Enum Members
Enum Member Enum Member Description Fit Current Saved -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-