BasePartBookmarkOption Enumeration¶
NXOpen.BasePart.BookmarkOption is an alias for NXOpen.BasePartBookmarkOption
-
class
NXOpen.
BasePartBookmarkOption
¶ Bases:
object
Controls the information written to a bookmark file.
In batch mode, the options:
BasePartBookmarkOption.AllPlusDisplay
BasePartBookmarkOption.ComponentGroupsLoadOptionsPlusDisplay
BasePartBookmarkOption.ComponentGroupsOnlyPlusDisplay
BasePartBookmarkOption.DisplayOnly
are not supported. They will be treated as if the option specfied were:BasePartBookmarkOption.All
BasePartBookmarkOption.ComponentGroupsLoadOptions
BasePartBookmarkOption.ComponentGroupsOnly
BasePartBookmarkOption.Empty
respectively.Enum Members
Enum Member Enum Member Description All Write component groups, load options and structure.ComponentGroupsLoadOptions Write component groups and load options.ComponentGroupsOnly Write component groups only.AllPlusDisplay Write component groups, load options, structure and display attributesComponentGroupsLoadOptionsPlusDisplay Write component groups, load options and display attributesComponentGroupsOnlyPlusDisplay Write component groups and display attributesDisplayOnly Write only display attributesEmpty Write nothing but header information-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-