SketchCopyObjectData_Struct Struct¶
NXOpen.Sketch.CopyObjectData is an alias for NXOpen.SketchCopyObjectData_Struct
-
class
NXOpen.
SketchCopyObjectData_Struct
¶ Bases:
object
This structure represents a map between the original object to be copied and the corresponding copied object.
An array of these structures are returned from the API
NXOpen.Sketch.CopyObjects()
. . Constructor: NXOpen.Sketch.CopyObjectData()
Fields¶
Field | Description |
---|---|
OrigObject | |
CopiedObject |
OrigObject¶
-
SketchCopyObjectData_Struct.
OrigObject
¶ -------------------------------------
Field Value Type:
NXOpen.NXObject
CopiedObject¶
-
SketchCopyObjectData_Struct.
CopiedObject
¶ -------------------------------------
Field Value Type:
NXOpen.NXObject