MassPropertiesBuilderUpdateOptions Enumeration¶
NXOpen.MassPropertiesBuilder.UpdateOptions is an alias for NXOpen.MassPropertiesBuilderUpdateOptions
-
class
NXOpen.
MassPropertiesBuilderUpdateOptions
¶ Bases:
object
Specifies the Update on Save option that will be applied to all selected objects.
Enum Members
Enum Member Enum Member Description No The Update on Save property will be turned off for all selected objects.Yes The Update on Save property will be turned on for all selected objects.Mixed The Update on Save property will not change for the selected objects.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-