AutomaticTraceline Class¶
-
class
NXOpen.
AutomaticTraceline
¶ Bases:
NXOpen.Traceline
Represents an automatic traceline.
This type of traceline has its shape automatically derived from its defining properties.
No creator defined due to apiwrap problems
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
EndDirection | Returns or sets the end direction of the traceline |
EndOffset | Returns or sets the end offset of the traceline |
EndPoint | Returns or sets the end point of the traceline |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Mode | Returns or sets the mode of the traceline |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
Orientation | Returns or sets the orientation of the traceline |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Solution | Returns or sets the solution used in the traceline |
StartDirection | Returns or sets the start direction of the traceline |
StartOffset | Returns or sets the start offset of the traceline |
StartPoint | Returns or sets the start point of the traceline |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AskExplosion | Returns the explosion that the traceline has been created in @return Explosion |
AskShape | Returns the object used to represent the shape of the traceline @return Traceline shape |
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSegmentConstraints | Gets the segment constraints of the traceline |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveSegmentConstraint | Removes the segment constraint from the traceline |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSegmentConstraints | Sets the segment constraints of the traceline |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Enumerations¶
AutomaticTracelineModeOption Enumeration | Controls the mode used when evaluating an automatic traceline |
Property Detail¶
EndDirection¶
-
AutomaticTraceline.
EndDirection
¶ Returns or sets the end direction of the traceline
-------------------------------------
Getter Method
Signature
EndDirection()
Returns: End direction Return type: NXOpen.Direction
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
EndDirection(direction)
Parameters: direction ( NXOpen.Direction
) – New end directionNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
EndOffset¶
-
AutomaticTraceline.
EndOffset
¶ Returns or sets the end offset of the traceline
-------------------------------------
Getter Method
Signature
EndOffset()
Returns: End offset Return type: float New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
EndOffset(endOffset)
Parameters: endOffset (float) – New end offset New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
EndPoint¶
-
AutomaticTraceline.
EndPoint
¶ Returns or sets the end point of the traceline
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: End point Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
EndPoint(point)
Parameters: point ( NXOpen.Point
) – New end pointNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
IsOccurrence¶
-
AutomaticTraceline.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
AutomaticTraceline.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Mode¶
-
AutomaticTraceline.
Mode
¶ Returns or sets the mode of the traceline
-------------------------------------
Getter Method
Signature
Mode()
Returns: Mode Return type: NXOpen.AutomaticTracelineModeOption
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
Mode(mode)
Parameters: mode ( NXOpen.AutomaticTracelineModeOption
) – New modeNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Name¶
-
AutomaticTraceline.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Orientation¶
-
AutomaticTraceline.
Orientation
¶ Returns or sets the orientation of the traceline
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Orientation Return type: NXOpen.Matrix3x3
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
Orientation(orientation)
Parameters: orientation ( NXOpen.Matrix3x3
) – New orientationNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
OwningComponent¶
-
AutomaticTraceline.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
AutomaticTraceline.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
AutomaticTraceline.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Solution¶
-
AutomaticTraceline.
Solution
¶ Returns or sets the solution used in the traceline
-------------------------------------
Getter Method
Signature
Solution()
Returns: Solution used Return type: int New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
Solution(solution)
Parameters: solution (int) – New solution to use New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
StartDirection¶
-
AutomaticTraceline.
StartDirection
¶ Returns or sets the start direction of the traceline
-------------------------------------
Getter Method
Signature
StartDirection()
Returns: Start direction Return type: NXOpen.Direction
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
StartDirection(direction)
Parameters: direction ( NXOpen.Direction
) – New start directionNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
StartOffset¶
-
AutomaticTraceline.
StartOffset
¶ Returns or sets the start offset of the traceline
-------------------------------------
Getter Method
Signature
StartOffset()
Returns: Start offset Return type: float New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
StartOffset(startOffset)
Parameters: startOffset (float) – New start offset New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
StartPoint¶
-
AutomaticTraceline.
StartPoint
¶ Returns or sets the start point of the traceline
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Start point Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
-------------------------------------
Setter Method
Signature
StartPoint(point)
Parameters: point ( NXOpen.Point
) – New start pointNew in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
FindObject¶
-
AutomaticTraceline.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetSegmentConstraints¶
-
AutomaticTraceline.
GetSegmentConstraints
¶ Gets the segment constraints of the traceline
Signature
GetSegmentConstraints()
Returns: a tuple Return type: A tuple consisting of (segmentIndices, segmentLengths). segmentIndices is a list of int. Segment indices segmentLengths is a list of float. Segment lengths New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Print¶
-
AutomaticTraceline.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveSegmentConstraint¶
-
AutomaticTraceline.
RemoveSegmentConstraint
¶ Removes the segment constraint from the traceline
Signature
RemoveSegmentConstraint(segmentIndex)
Parameters: segmentIndex (int) – Segment index New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
SetName¶
-
AutomaticTraceline.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSegmentConstraints¶
-
AutomaticTraceline.
SetSegmentConstraints
¶ Sets the segment constraints of the traceline
Signature
SetSegmentConstraints(segmentIndices, segmentLengths)
Parameters: - segmentIndices (list of int) – Segment indices
- segmentLengths (list of float) – Segment lengths
New in version NX4.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)