PartCollectionSetProtectionOn Enumeration¶
NXOpen.PartCollection.SetProtectionOn is an alias for NXOpen.PartCollectionSetProtectionOn
-
class
NXOpen.
PartCollectionSetProtectionOn
¶ Bases:
object
Specifies the parts to which the password protection operation will apply.
This structure should only be used with GC Toolkits.
Enum Members
Enum Member Enum Member Description DisplayedPart The Displayed partDisplayedPartandComponents All fully open parts in the sessionAllParts Displayed part and full open components of the part-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-