STLImporterFileFormatType Enumeration¶
NXOpen.STLImporter.FileFormatType is an alias for NXOpen.STLImporterFileFormatType
-
class
NXOpen.
STLImporterFileFormatType
¶ Bases:
object
Specifies the STL file format.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Ascii STL file is in ASCII format.Binary STL file is in binary format.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-