AcisExporter Class¶
-
class
NXOpen.
AcisExporter
¶ Bases:
NXOpen.Builder
Represents a
AcisExporter
to be used when importing the Acis Data This class is created usingDexManager
. NULL object will be returned from Commit()To create a new instance of this class, use
NXOpen.DexManager.CreateAcisExporter()
Default values.
Property Value AcisVersion R18 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AcisVersion | Returns or sets the Acis version - The version of ACIS file to be exported |
ExportSelectionBlock | Returns the export selection block - the object selection will be done by this block. |
FileSaveFlag | Returns or sets the file save flag - this should be set to false if doing File Export |
OutputFile | Returns or sets the output file - the exported data will be written to file specified |
SettingsFile | Returns or sets the settings file - The definition file to read default options |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SaveSettings | Save the settings - this will save the settings to a file sepcified |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AcisExporterAcisVersionOption Enumeration | ACIS Version options |
Property Detail¶
AcisVersion¶
-
AcisExporter.
AcisVersion
¶ Returns or sets the Acis version - The version of ACIS file to be exported
-------------------------------------
Getter Method
Signature
AcisVersion()
Returns: Return type: NXOpen.AcisExporterAcisVersionOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AcisVersion(acisVersion)
Parameters: acisVersion ( NXOpen.AcisExporterAcisVersionOption
) –New in version NX11.0.0.
License requirements: None.
ExportSelectionBlock¶
-
AcisExporter.
ExportSelectionBlock
¶ Returns the export selection block - the object selection will be done by this block.
-------------------------------------
Getter Method
Signature
ExportSelectionBlock()
Returns: Return type: NXOpen.ObjectSelector
New in version NX11.0.0.
License requirements: None.
FileSaveFlag¶
-
AcisExporter.
FileSaveFlag
¶ Returns or sets the file save flag - this should be set to false if doing File Export
-------------------------------------
Getter Method
Signature
FileSaveFlag()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileSaveFlag(doingFileSave)
Parameters: doingFileSave (bool) – New in version NX11.0.0.
License requirements: None.
OutputFile¶
-
AcisExporter.
OutputFile
¶ Returns or sets the output file - the exported data will be written to file specified
-------------------------------------
Getter Method
Signature
OutputFile()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputFile(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: None.
SettingsFile¶
-
AcisExporter.
SettingsFile
¶ Returns or sets the settings file - The definition file to read default options
-------------------------------------
Getter Method
Signature
SettingsFile()
Returns: Return type: str New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SettingsFile(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: None.
Method Detail¶
SaveSettings¶
-
AcisExporter.
SaveSettings
¶ Save the settings - this will save the settings to a file sepcified
Signature
SaveSettings(filename)
Parameters: filename (str) – New in version NX11.0.0.
License requirements: None.
Validate¶
-
AcisExporter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.