SessionProjectAssignmentState Enumeration¶
NXOpen.Session.ProjectAssignmentState is an alias for NXOpen.SessionProjectAssignmentState
-
class
NXOpen.
SessionProjectAssignmentState
¶ Bases:
object
Indicates project assignment state
Enum Members
Enum Member Enum Member Description NotSet to remove project from all objectsPartial to skip project assignmentFull to assign project to all objects-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-