FontCollection Class¶
-
class
NXOpen.
FontCollection
¶ Bases:
object
Represents a collection of typographical fonts (for example, Arial, OldEnglish)
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
AddFont | Adds a font to the part. |
DoesFontExist | Finds out whether the specified ID is associated with a font @return True iff the font exists |
GetFontName | Returns the name for the font that has the specified integer ID @return The font’s name |
GetFontType | Returns the font type of the font at the provided index @return Type of the font |
GetLength | Returns the number of fonts in the part @return |
ReplaceFont | Replaces a font name and type at the given font index |
Enumerations¶
FontCollectionType Enumeration | Specifies the type of font |
Method Detail¶
AddFont¶
-
FontCollection.
AddFont
¶ Overloaded method AddFont
AddFont(fontName)
AddFont(fontName, type)
-------------------------------------
Adds a font to the part. This will only add NX fonts. To add Standard fonts, use the overloaded
FontCollection.AddFont()
routine that accepts the font type. If the font name already exists in the part, this will return the existing font index.Signature
AddFont(fontName)
Parameters: fontName (str) – Font name Returns: Integer ID that the method assigns to the font Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Adds a font to the part. This can be used to create both NX and Standard fonts. If the font name already exists in the part, this will return the existing font index.
Signature
AddFont(fontName, type)
Parameters: - fontName (str) – Font name
- type (
NXOpen.FontCollectionType
) – Type of the font
Returns: Integer ID that the method assigns to the font
Return type: int
New in version NX7.5.0.
License requirements: None.
-------------------------------------
DoesFontExist¶
-
FontCollection.
DoesFontExist
¶ Finds out whether the specified ID is associated with a font
Signature
DoesFontExist(fontIndex)
Parameters: fontIndex (int) – ID of the font Returns: True iff the font exists Return type: bool New in version NX3.0.0.
License requirements: None.
GetFontName¶
-
FontCollection.
GetFontName
¶ Returns the name for the font that has the specified integer ID
Signature
GetFontName(fontIndex)
Parameters: fontIndex (int) – The ID for the font Returns: The font’s name Return type: str New in version NX3.0.0.
License requirements: None.
GetFontType¶
-
FontCollection.
GetFontType
¶ Returns the font type of the font at the provided index
Signature
GetFontType(fontIndex)
Parameters: fontIndex (int) – ID of the font Returns: Type of the font Return type: NXOpen.FontCollectionType
New in version NX7.5.0.
License requirements: None.
GetLength¶
-
FontCollection.
GetLength
¶ Returns the number of fonts in the part
Signature
GetLength()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
ReplaceFont¶
-
FontCollection.
ReplaceFont
¶ Replaces a font name and type at the given font index
Signature
ReplaceFont(fontIndex, type, fontName)
Parameters: - fontIndex (int) – ID of the font
- type (
NXOpen.FontCollectionType
) – New type of the font - fontName (str) – New name of the font
New in version NX7.5.0.
License requirements: None.