AttributeManager Class¶
-
class
NXOpen.
AttributeManager
¶ Bases:
object
Provides methods for querying and updating attributes.
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateAttributePropertiesBuilder | Creates the AttributePropertiesBuilder @return |
Method Detail¶
CreateAttributePropertiesBuilder¶
-
AttributeManager.
CreateAttributePropertiesBuilder
¶ Creates the AttributePropertiesBuilder
Signature
CreateAttributePropertiesBuilder(part, objects, operationType)
Parameters: - part (
NXOpen.BasePart
) – The part that owns the builder. The builder owner is not strictly required (that is, it can be None), but it is highly suggested to ensure proper cleanup of the builder in case the client does not explicitly clean it up properly. - objects (list of
NXOpen.NXObject
) – the array of objects - operationType (
NXOpen.AttributePropertiesBuilderOperationType
) – the type of operation
Returns: Return type: New in version NX8.5.0.
License requirements: None.
- part (