PartLoadStatus Class

class NXOpen.PartLoadStatus

Bases: NXOpen.TransientObject

Represents a list of part names with associated status codes.

The status codes serve to communicate why these parts were not able to be loaded during part open.

Note that if an exception is thrown during the load process, the load status structure will not be usable as the load process itself has failed and nothing will have been loaded. This load status can only be used for partially successful load operations and some load warnings.

New in version NX3.0.0.

Properties

Property Description
NumberUnloadedParts Returns the number of parts that could not be loaded.

Methods

Method Description
Dispose Free resources associated with the instance.
GetPartName Returns the name of a particular part that could not be loaded.
GetStatus Returns the status code for a part that could not be loaded.
GetStatusDescription Returns the text description of the status code for a part that could not be loaded.

Property Detail

NumberUnloadedParts

PartLoadStatus.NumberUnloadedParts

Returns the number of parts that could not be loaded.

-------------------------------------

Getter Method

Signature NumberUnloadedParts()

Returns:
Return type:int

New in version NX3.0.0.

License requirements: None.

Method Detail

Dispose

PartLoadStatus.Dispose

Free resources associated with the instance.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX3.0.0.

License requirements: None.

GetPartName

PartLoadStatus.GetPartName

Returns the name of a particular part that could not be loaded.

Signature GetPartName(i)

Parameters:i (int) – Index into list of unloaded parts
Returns:
Return type:str

New in version NX3.0.0.

License requirements: None.

GetStatus

PartLoadStatus.GetStatus

Returns the status code for a part that could not be loaded.

Signature GetStatus(i)

Parameters:i (int) – Index into list of unloaded parts
Returns:
Return type:int

New in version NX3.0.0.

License requirements: None.

GetStatusDescription

PartLoadStatus.GetStatusDescription

Returns the text description of the status code for a part that could not be loaded.

Signature GetStatusDescription(i)

Parameters:i (int) – Index into list of unloaded parts.
Returns:
Return type:str

New in version NX3.0.0.

License requirements: None.