HumanDataInverseKinematicsHeadEyeType Enumeration¶
NXOpen.HumanData.InverseKinematicsHeadEyeType is an alias for NXOpen.HumanDataInverseKinematicsHeadEyeType
-
class
NXOpen.
HumanDataInverseKinematicsHeadEyeType
¶ Bases:
object
This enum represents the head and eye type of active reach
Enum Members
Enum Member Enum Member Description FollowLastDefined Indicate the position of head and eye follow the last defined positionFixate Indicate the position of head and eye is fixate-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-