ValidationInputType Enumeration¶
NXOpen.Validation.InputType is an alias for NXOpen.ValidationInputType
-
class
NXOpen.
ValidationInputType
¶ Bases:
object
Specifies the input type
Enum Members
Enum Member Enum Member Description KfClass Input rules are in a KF classSpreadsheet Input rules are from a spreadsheetTextFile Input rules are from a text fileXml Input rules are from XML fileTcr Input rules are from TcRApplication Input rules are from validation applicationsNum Last item define the number of the input source, not used as a type.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-