SketchConstraintPointType Enumeration¶
NXOpen.Sketch.ConstraintPointType is an alias for NXOpen.SketchConstraintPointType
-
class
NXOpen.
SketchConstraintPointType
¶ Bases:
object
Used in ConstraintGeometry to indicate what type of point, if any, the geometry is
Enum Members
Enum Member Enum Member Description NotSet The geometry is not a pointStartVertex Start vertex (e.g. the start point of a line)EndVertex End vertex (e.g. the end point of a line)ArcCenter Center of a circle, arc, or ellipseSplineDefiningPoint A defining point of a spline.Anchor The anchor point of a conicSplinePole The control pole of a splineMidVertex The mid vertex of a line or an arc-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-