EdgeIntersectRule Class¶
-
class
NXOpen.
EdgeIntersectRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects all intersection edges between a set of faces.New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the edge intersect rule: NXOpen.EdgeIntersectRule |
Method Detail¶
Dispose¶
-
EdgeIntersectRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX3.0.0.
License requirements: None.
GetData¶
-
EdgeIntersectRule.
GetData
¶ Gets the data for the edge intersect rule:
NXOpen.EdgeIntersectRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (facesOfFeatures1, facesOfFeatures2). facesOfFeatures1 is a list of
NXOpen.Face
. Faces of feature1 whose boundary edges are used to create this rule.facesOfFeatures2 is a list ofNXOpen.Face
. Faces of feature2 whose boundary edges are used to create this rule. .. versionadded:: NX3.0.0License requirements: gateway (“UG GATEWAY”)