RuleManagerInitializationStatusType Enumeration¶
NXOpen.RuleManager.InitializationStatusType is an alias for NXOpen.RuleManagerInitializationStatusType
-
class
NXOpen.
RuleManagerInitializationStatusType
¶ Bases:
object
Indicates the status from initializing RuleManager.
Enum Members
Enum Member Enum Member Description Success Initialization succeededFailure Initialization failedUnavailable Intent not availableUnableToObtainLicense Cannot obtain licenseCloseFailure Close failed-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-