PrintPDFBuilderOutputTextOption Enumeration¶
NXOpen.PrintPDFBuilder.OutputTextOption is an alias for NXOpen.PrintPDFBuilderOutputTextOption
-
class
NXOpen.
PrintPDFBuilderOutputTextOption
¶ Bases:
object
Specifies the output text option, as either text or polylines
Enum Members
Enum Member Enum Member Description Text Text is kept as textPolylines Text is exported as polylines-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-