PartImporter Class¶
-
class
NXOpen.
PartImporter
¶ Bases:
NXOpen.Importer
Used to import a part into the work part.
The imported part can be an NX part or a foreign part, e.g. an I-DEAS, CATIA, or Teamcenter Visualization part. A named group will be created with the contents of the imported part if the property
NXOpen.PartImporter.CreateNamedGroup`()
is turned on. You can access the named group which is created when importing the part by accessing the object array returned from the methodBuilder.GetCommittedObjects()
after you execute theBuilder.Commit()
on theNXOpen.PartImporter
.To obtain an instance of this class use
ImportManager.CreatePartImporter()
.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CreateNamedGroup | Returns or sets the Create Named Group flag. |
DestinationCoordinateSystem | Returns or sets the destination coordinate system. |
DestinationCoordinateSystemSpecification | Returns or sets the destination coordinate system specification. |
DestinationPoint | Returns or sets the destination point. |
FileName | Returns or sets the name of the file containing the data to import. |
ImportCamObjects | Returns or sets the Import CAM Objects flag. |
ImportViews | Returns or sets the Import Views flag. |
LayerOption | Returns or sets the layer option. |
Scale | Returns or sets the scale. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetSpecifiedCoordinateSystem | Sets the specified coordinate system. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PartImporterDestinationCoordinateSystemSpecificationType Enumeration | Specifies the destination coordinate system specification. |
PartImporterLayerOptionType Enumeration | Specifies on which layer to import a part. |
Property Detail¶
CreateNamedGroup¶
-
PartImporter.
CreateNamedGroup
¶ Returns or sets the Create Named Group flag.
True if the Create Named Group flag is on.
-------------------------------------
Getter Method
Signature
CreateNamedGroup()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateNamedGroup(createNamedGroup)
Parameters: createNamedGroup (bool) – New in version NX5.0.0.
License requirements: None.
DestinationCoordinateSystem¶
-
PartImporter.
DestinationCoordinateSystem
¶ Returns or sets the destination coordinate system.
-------------------------------------
Getter Method
Signature
DestinationCoordinateSystem()
Returns: Return type: NXOpen.NXMatrix
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationCoordinateSystem(destinationCoordinateSystem)
Parameters: destinationCoordinateSystem ( NXOpen.NXMatrix
) –New in version NX5.0.0.
License requirements: None.
DestinationCoordinateSystemSpecification¶
-
PartImporter.
DestinationCoordinateSystemSpecification
¶ Returns or sets the destination coordinate system specification.
-------------------------------------
Getter Method
Signature
DestinationCoordinateSystemSpecification()
Returns: Return type: NXOpen.PartImporterDestinationCoordinateSystemSpecificationType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationCoordinateSystemSpecification(destinationCoordinateSystemSpecification)
Parameters: destinationCoordinateSystemSpecification ( NXOpen.PartImporterDestinationCoordinateSystemSpecificationType
) –New in version NX5.0.0.
License requirements: None.
DestinationPoint¶
-
PartImporter.
DestinationPoint
¶ Returns or sets the destination point.
-------------------------------------
Getter Method
Signature
DestinationPoint()
Returns: Return type: NXOpen.Point3d
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationPoint(destinationPoint)
Parameters: destinationPoint ( NXOpen.Point3d
) –New in version NX5.0.0.
License requirements: None.
ImportCamObjects¶
-
PartImporter.
ImportCamObjects
¶ Returns or sets the Import CAM Objects flag.
True if the Import CAM Objects flag is on.
-------------------------------------
Getter Method
Signature
ImportCamObjects()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportCamObjects(importCamObjects)
Parameters: importCamObjects (bool) – New in version NX5.0.0.
License requirements: None.
ImportViews¶
-
PartImporter.
ImportViews
¶ Returns or sets the Import Views flag.
True if the Import Views flag is on.
-------------------------------------
Getter Method
Signature
ImportViews()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImportViews(importViews)
Parameters: importViews (bool) – New in version NX5.0.0.
License requirements: None.
LayerOption¶
-
PartImporter.
LayerOption
¶ Returns or sets the layer option.
-------------------------------------
Getter Method
Signature
LayerOption()
Returns: Return type: NXOpen.PartImporterLayerOptionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LayerOption(layerOption)
Parameters: layerOption ( NXOpen.PartImporterLayerOptionType
) –New in version NX5.0.0.
License requirements: None.
Scale¶
-
PartImporter.
Scale
¶ Returns or sets the scale.
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
SetSpecifiedCoordinateSystem¶
-
PartImporter.
SetSpecifiedCoordinateSystem
¶ Overloaded method SetSpecifiedCoordinateSystem
SetSpecifiedCoordinateSystem(specifiedCoordinateSystem)
SetSpecifiedCoordinateSystem(specifiedCoordinateSystem, deleteSpecifiedCoordinateSystem)
-------------------------------------
Sets the specified coordinate system. This specified coordinate system is deleted after setting the destination coordinate system
Signature
SetSpecifiedCoordinateSystem(specifiedCoordinateSystem)
Parameters: specifiedCoordinateSystem ( NXOpen.CoordinateSystem
) –New in version NX8.0.0.
License requirements: None.
-------------------------------------
Sets the specified coordinate system. This provides an option whether to delete the specified coordinate system. If not mark for delete then it is user’s responsibility to delete the specified coordinate system.
Signature
SetSpecifiedCoordinateSystem(specifiedCoordinateSystem, deleteSpecifiedCoordinateSystem)
Parameters: - specifiedCoordinateSystem (
NXOpen.CoordinateSystem
) – - deleteSpecifiedCoordinateSystem (bool) – If true, the specified coordinate system is deleted.
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Validate¶
-
PartImporter.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.