PartImporterLayerOptionType Enumeration¶
NXOpen.PartImporter.LayerOptionType is an alias for NXOpen.PartImporterLayerOptionType
-
class
NXOpen.
PartImporterLayerOptionType
¶ Bases:
object
Specifies on which layer to import a part.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description Work Import part on work layer.Original Import part on original layers.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-