SketchTrimInputOption Enumeration¶
NXOpen.Sketch.TrimInputOption is an alias for NXOpen.SketchTrimInputOption
-
class
NXOpen.
SketchTrimInputOption
¶ Bases:
object
Indicates whether the input curves should be trimmed when doing a fillet
Enum Members
Enum Member Enum Member Description False Do not trim the input curvesTrue Trim the input curves-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-